Feedback_Kalfas
| Index.Sub | 2230.0DH |
| Data Type | Unsigned16 |
| Access | Read/Write |
| PDO Mappable |
No |
| Unit |
-- |
|
Range |
Unsigned16 |
| Default Value |
0 |
| Store Supported | Yes |
| Description |
This value is used for Closed Loop feature. It is used to change the advance angle depending by speed. |
|
Notes |
For speed value higher than 1500 rpm, set value equal to 60000. |